Hi,
I have Windows 7 service pack 1 and CCS 6.0.0.00190
I'm attempting to get a program I have written in C to run on the TMS320C6713 DSK. I have read through this guide: http://processors.wiki.ti.com/index.php/C6713DSK_in_CCSv5
When I try to do the Prerequisite steps, the 6713DSK Diagnostics fails with this error.
Starting diagnostic test suite.
--> Running USB diagnostics.
Can't connect to target.
*** Plug in power and USB cable.
*** Can't run if Code Composer or Diagnostic already running.
Result> USB diagnostic fail
Stopping diagnostic suite.
It works on another computer that is running XP, but CCS v6 will not run on that machine. My question is does the Diagnostic executable have to pass the tests for the emulation to work correctly, or may I simply proceed to use the board normally with CCS?