I am trying to install CCS for use with a Tiva C Series Launchpad, but the links I have do not seem to provide any option to specify the 64-bit OS. I killed the firewall and anti-virus and the install ram OK, but the install file is labeled win32 and the config file contains a number of references to Win32, but none to Win64. I assume that the installed CCS is in fact 32-bit.
I tried out several of the demo programs on the Launchpad since some other 32-bit applications do work on this system. The CCS runs OK. The demos compile and load, but have memory access failures when run.
My question is how can I locate, download and install the real 64-bit CCS?