I am using CCS 5.5.0.00077 with a Spectrum Digital XDS560V2 STM LAN emulator. My target contains a 66AK2H12. I can connect to all the DSP C66xx and ARM 15 cores. I am able to access memory using the memory browser from each core's view as expected as long as the address is 32-bit. I would like to verify DDR3A. When I enter the 40-bit address from the ARM core connection, a dialog pops up indicating that the address is out of range.
Is it possible to make 36-bit or 40-bit accesses from the memory browser?