Hey, I'm having issues with DSS while running code composer. I'm using a simple script to read from certain memory locations. This script has worked so far, except when code composer is currently debugging. In this case, initialization (openSession()) fails with "Error initializing emulator". I'm hoping to be able to use this script while debugging in CCS, so I can halt the proccessor at some point, then run the script to get values. The script is currently be run via the provided DSS batch file. It seems that I can mirror the functionality by manually calling into the DSS API from the eclipse scripting console, but when I launch from the batch I can't openSession(). Any idea what might cause this error? Is what I'm doing supported? I tried loading my js file from the scripting console, but there are issues I would need to work through, and this isn't ideal. I'm using v5.5 and a XDS510USB