Hi all,
After solving this issue (http://e2e.ti.com/support/development_tools/code_composer_studio/f/81/t/362148.aspx) with some help from Rafael, I have a new problem. Now, I can begin using the statistical function profiler, but when I hit Continue, or try to run to a breakpoint, TraceServer begins using 100% processor on one core.
At this point, Code Composer turns white and gets the 'spinning cursor' effect, but doesn't crash - just hangs while TraceServer uses 100% CPU. I have multiple cores, so it's not like I'm preventing Code Composer from getting CPU time just by having TraceServer pegged.
At this point, Code Composer is out to lunch and there seems to be no way to recover it. I end up having to close the entire program and power cycle the target.
Any ideas or suggestions?
Thanks,
Ben