Hi,
I am currently using CCS v5.1 (Full name = Version: 5.1.0.09000) with a blackhawk USB-2000 emulator and everything has been fine for the last 2 years.
However, the Blackhawk USB-2000 and been replaced by the USB-200 (yes they dropped a nought!)
My version of CCS (v5.1) doesnt have support for the USB-200.
Is it possible to add that support to my version of CCS, or do I have to upgrade to a newer version of CCS?
....In the case that I have to upgrade, can I transfer my license file? How do I do this? Is it a simple automatic upgrade or do I need to uninstall my current version and then install the new version?
...also I tried loading my CCS5.5 project into a colleagues PC with CCSv5.5 and the project would not load. What version of CCS would you recommend that I upgrade to that I can use my project file and also USB-200??
Thanks in advance!