Hi all. I a trying to program an msp430F5509 via spy-by-wire in ccs v5. it says it cannot connect to the target. Any help would be appreciated as i am new to ccs.
Dave
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi all. I a trying to program an msp430F5509 via spy-by-wire in ccs v5. it says it cannot connect to the target. Any help would be appreciated as i am new to ccs.
Dave
thanks Gautam. i have double checked my hardware and it's fine. I am multiplexing the TDIO/RST pin with a reset push-button. could this be a problem?
David Holbeche said:I am multiplexing the TDIO/RST pin with a reset push-button. could this be a problem?
David, here's your device specific interface for Spy-bi-wire:
http://e2e.ti.com/support/microcontrollers/msp430/f/166/t/248561.aspx
Regards,
Gautam
Hi David,
what FET are you using? What OS? The new small black msp FET only works with v6 of CCS.
A couple further quick things. Have you tried a different cable or port? Have you been able to try on a different pc?
Best regards,
Lisa
Dear Gautam,
thanks for the reply i will test it on monday without the 47K and the 330R resistors and add the 2.2 nF cap which was missing.
Dave
David Holbeche said:thanks for the reply i will test it on monday without the 47K and the 330R resistors and add the 2.2 nF cap which was missing.
Sure Dave, do keep us informed.
Regards,
Gautam
Hi Gautam. It's working now on another machine . i removed the 330R and had a large capacitance on the RST pin which was also removed. I think these were the issues. thanks for everyone's help =)
Dave