Hi all,
I'm a new in CCS and TMS320F2812.
I have QQ2812 v1.3 target board and emulator xds100v2. I'm developing uint tests for a firmware. All works perfetly. Tests are flashed to chip and run succsesfully.
I use CCS 3.3 and F28xx On-Chip Flash Programmer plugin to flash microcontroller F2812 manually. I have a hundred tests and it's necessary to run all of them each time when new firmware released. So it does mannually takes a long time.
So the question is how to automatically flash the chip via command line utility or gel file and detect the moment when test is finished and to start flashing other test?
Thank you,
The best regards,
Alex