Hello Experts,
I have CCSv5 and CCSv6 installed on my linux host(ubuntu 12.04). I have K2HEVM.
I have created target configuration file to connect with cores and tested the connection. All passed.
Case 1:
I have selected all DSP cores(0-7) and click on "Connnect target". The CCS crashed. Please find the CCS err log file and console screenshot.
1. CCS Log: 2818.8715.hs_err_pid28164.log
Case 2:
I have selected DSP cores(0-6) and click on "Connnect target". The CCS is able to connect with all selected cores. When I try to load the .out file on selected cores. The CCS throws "Load program error" message after loading out file on 5 cores.
After above my host machine hangs. When i restarted the CCS, I am not able to emulator connect with dsp core. It is always failing.
There is no issue with out file. The out file is working on any single dsp core. I have attached the out file for your reference.
4666.7725.helloWorld_evmk2h.out
Please help to resolve above issues.
Note: These issue are observed only on Linux version of CCS. We observe this issue with both CCS 5 & 6.
Thank you.