Hi, I'm currently practicing on some examples as I'm new, and I faced an issue which I'm not sure how to solve, hope u guys can help.
CCS: ccsv5
Board: TMDXEVM6678LE
Problem:
I previously wrote two piece of code, one which sends UDP message and the other receives and displays the messages. I'm trying to load the sending code into the DSP so that it can send messages while my desktop receives.
But currently it seems that I'm only able to receive the latest message sent. Eg:
Core.send(reinterpret_cast<char*>(&sendData1), sizeof(sendData1), "192.168.x.xxx", 50001);
Core.send(reinterpret_cast<char*>(&sendData2), sizeof(sendData2), "192.168.x.xxx", 50001);
Only sendData2 will be sent/received, I've also tried adding a delay between send but doesn't seem to solve. I was wondering if anyone here would have any knowledge or advice on how I could solve this.
PS: I'm sorry of my description of the problem is vague, I'll try to provide more information if requested, as I'm not sure what is required. Typing this from my phone as there's no internet on the PC T_T