Hello
I recently upgraded my OS to Ubuntu 14.04 Trusty, and I installed Code Composer Studio v6.0.1. When I start CSS6, it crashed with the following message (extract):
# An unexpected error has been detected by Java Runtime Environment:
#
# SIGSEGV (0xb) at pc=0x85aa3edf, pid=3094, tid=3075888896
#
# Java VM: Java HotSpot(TM) Client VM (11.3-b02 mixed mode linux-x86)
# Problematic frame:
# C [libwebkitgtk-1.0.so.0+0x1d0edf]
#
I obtain the same error with oracle-java7, oracle-java8 or openjdk7. What surprises me is the version of Java Hotspot (11.3-b02) whereas:
$ java -version
java version "1.7.0_67"
Java(TM) SE Runtime Environment (build 1.7.0_67-b01)
Java HotSpot(TM) Server VM (build 24.65-b04, mixed mode)
$ echo $JAVA_HOME
/usr/lib/jvm/java-7-oracle
Where and why does CCS6 find this old VM?
Yves Grenier