Dear TI team,
I am using Zeiss DM6446-wifi Evaluation Module with CCS v5.3. The projects for the same processor is available from Spectrum Digital Website. I have downloaded the projects,they are built using CCS v3.3.I am trying to import the project in CCSv5.3. The project gets imported succesfully. Screenshot is as follows
If I try to load .out file for this project, it works fine, But if I Rebuild the project, it shows compilation failure.
The errors are
The console displays
**** Build of configuration Debug for project video_loopback ****
"C:\\ti\\ccsv5\\utils\\bin\\gmake" -k all
'Building file: ../main.c'
'Invoking: ARM Compiler'
"C:/ti/ccsv5/tools/compiler/arm_5.0.1/bin/armcl" -mv5e --code_state=32 --abi=ti_arm9_abi -me -O1 -g --include_path="C:/ti/ccsv5/tools/compiler/arm_5.0.1/include" --include_path="C:/ti/xdais_7_21_01_07/packages/ti/xdais" --include_path=".." --include_path="C:/Users/saraswati/Desktop/BIG_DATA/DM6446_DATA/dm6446/davincievm/davincievm/include" --include_path="C:/Users/saraswati/Desktop/BIG_DATA/DM6446_DATA/dm6446/davincievm/davincievm/csl/arm/inc" --define="_DEBUG" --define="ARM_SIDE" --define=dm6446 --quiet --display_error_number --preproc_with_compile --preproc_dependency="main.pp" "../main.c"
"../main.c", line 38: warning #1119-D: this assembly directive potentially unsafe inside a function
"../main.c", line 62: warning #1119-D: this assembly directive potentially unsafe inside a function
'Finished building: ../main.c'
' '
'Building file: ../video_test.c'
'Invoking: ARM Compiler'
"C:/ti/ccsv5/tools/compiler/arm_5.0.1/bin/armcl" -mv5e --code_state=32 --abi=ti_arm9_abi -me -O1 -g --include_path="C:/ti/ccsv5/tools/compiler/arm_5.0.1/include" --include_path="C:/ti/xdais_7_21_01_07/packages/ti/xdais" --include_path=".." --include_path="C:/Users/saraswati/Desktop/BIG_DATA/DM6446_DATA/dm6446/davincievm/davincievm/include" --include_path="C:/Users/saraswati/Desktop/BIG_DATA/DM6446_DATA/dm6446/davincievm/davincievm/csl/arm/inc" --define="_DEBUG" --define="ARM_SIDE" --define=dm6446 --quiet --display_error_number --preproc_with_compile --preproc_dependency="video_test.pp" "../video_test.c"
'Finished building: ../video_test.c'
' '
'Building target: video_loopback.out'
'Invoking: ARM Linker'
"C:/ti/ccsv5/tools/compiler/arm_5.0.1/bin/armcl" -mv5e --code_state=32 --abi=ti_arm9_abi -me -O1 -g --define="_DEBUG" --define="ARM_SIDE" --define=dm6446 --quiet --display_error_number -z --stack_size=0x800 -m"video_loopback.map" --heap_size=0x800 -i"C:/ti/ccsv5/tools/compiler/arm_5.0.1/lib" -i"C:/ti/ccsv5/tools/compiler/arm_5.0.1/include" -i"C:/Users/saraswati/Desktop/DM644x/video_loopback" -i"C:/Users/saraswati/Desktop/BIG_DATA/DM6446_DATA/dm6446/davincievm/davincievm/examples/video_loopback" --reread_libs --warn_sections --display_error_number --rom_model -o "video_loopback.out" "./video_test.obj" "./main.obj" -l"rts32e.lib" "../video.cmd"
error #10008-D: cannot find file "..\..\csl\arm\lib\Debug\csl_davinciArm9.lib"
error #10008-D: cannot find file "..\..\lib\davincievmbsl.lib"
undefined first referenced
symbol in file
--------- ----------------
_DAVINCIEVM_I2C_read ./video_test.obj
_DAVINCIEVM_I2C_write ./video_test.obj
_DAVINCIEVM_init ./main.obj
_DAVINCIEVM_waitusec ./video_test.obj
error #10234-D: unresolved symbols remain
error #10010: errors encountered during linking; "video_loopback.out" not
built
gmake: *** [video_loopback.out] Error 1
gmake: Target `all' not remade because of errors.
>> Compilation failure
**** Build Finished ****
NOW,as per my understanding even if I sppecify both the library paths in the project properties it shows error.
kindly suggest.
Thank you