Hi,
I'm using CCS6 with the TMS5701227. In the code below, I can't set a breakpoint on the if statement, CCS moves the breakpoint inside of the if block. If I put a breakpoint on the line before the if, it gets hit, but when I step through, it jumps to the line after the if block, like it is skipping the if statement all together.
pTask3RspMbox = OSMboxCreate(0); //Check to see if Mbox did not create.If it did not create successfully, a message is //sent to the fib diagnostic port and if running in debug assert is tripped and breaks code, but does not //print anything to a console window. if(pTask3RspMbox == 0) { diagPrintf("Error: FAILED To Create Task3 Rsp Mailbox\n\r"); OSTimeDly(10); ASSERT(pTask3RspMbox != 0); } initCAN();