my platform is CCS3.3, C6747, bios v5.41, code generation v6.11.
To find the reason of program fleet, I just want to monitor the value change of sepical RAM region
and PC jump to sepcial RAM region, for example: sepical RAM region is address 0x8000 to 0x9000, when value of address change I should get some tips or printf or breakpoint or something else, when PC jump to address get same thing too.
can the ccs plugin or tools can achieve those above or I must write some code to my progam to
achieve my thought.
urgent help, thank you.