I just need to do one simple thing, take a program i have been supplied and load it into the hardware (MSP430), why does it look like CCS does not even do this ?????
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I just need to do one simple thing, take a program i have been supplied and load it into the hardware (MSP430), why does it look like CCS does not even do this ?????
Hello Simon,
You can create a project-less debug session:
http://processors.wiki.ti.com/index.php/Projectless_Debug
Then you can load your program via 'Run -> Load -> Load Program'
Thanks
ki
Simon,
There are a number of ways to do this. If you just want to flash the program without debugging afterwards then loadti or Uniflash are better suited.
If you are looking to debug in CCS after loading then this is what I would do.
In CCS to to View -> Target Configurations.
Click on the button to create a new target configuration. Select your MSP430 device and the MSP430 USB FET as the connection. Save. This tells CCS what your hardware setup looks like.
In the target configuration view the file you just created will be listed under "User Defined". Right click on it and select to launch it. This will launch the debugger. you can then click on the connect button to connect and then the load button to specify the program to load.
You can make that target configuration file the default if you are always debugging the same device.
If you are doing this a lot you can set it up so that ti will connect and load automatically. After you have done the above once if you click on the down arrow beside the bug button select Debug Configurations. In the list on the left should be an item that matches the name of the target configuration file you created above. Select it.
Now you can set the program for it to load automatically:
You also want it to setup to automatically connect to the target otherwise the load will fail:
Now you can click on the down arrow beside the bug button and you should see the target config file name in the list and be able to just select it and it will launch the debugger, connect to the target and then load your program.
CCS is a development environment. If you just want to load and run without and feedback in a debugger I would suggest Uniflash or the loadti script that comes with Debug Server Scripting.
Regards,
John
Simon Turner1 said:open the project up, change program values and then compile and load the program into the target MCU (a version of MSP430)
Check out the CCS getting started video:
https://www.youtube.com/watch?v=uAb5MScflEo
From 2:50 to about 5:00, it shows a project in CCS and how to build the project and load the program to a target (MSP430).
The only difference in your case is you want to be able to open an existing project first by importing it into the workspace:
http://processors.wiki.ti.com/index.php/Projects_and_Build_Handbook_for_CCS#Importing_projects
And maybe modify some build properties
http://processors.wiki.ti.com/index.php/Projects_and_Build_Handbook_for_CCS#Project_Properties
Thanks
ki
Simon Turner1 said:So basically debug = program, if I hit F11 it will compile and load.
Basically, yes.
It actually does a little more. The full list of actions it does is:
-Prompt to save source files
-Build the project (incrementally)
-Start the debugger (CCS will switch to the CCS Debug perspective)
-Connect CCS to the target
-Load/Flash the program on the target
-Run to 'main'
Note that the above default actions are configurable (i.e. if you want to disable the 'run to main' action after program load, you can do so).
ok well it's the simplest thing to do i suppose, tell my boss to open the project and hit F11 after the program loads he needs to stop the debugging session and possibly terminate the connection.
If the debug session is stopped will the MCU run it's program normally without the "conection2 being terminated ?
if you shut down the debug session while the target is halted, the target will not resume execution. You will need to resume execution before terminating the debug session.