I have recently upgraded to CCS 6.0.1.00040 on Windows 7, 64 bit.
Although I have full license I also have tried to work with MSP-GCC 4.9.1, the migration was terrific.
But my real problem is the following: every time I compile with MSPGCC, the Problem window is always full of errors. It seemed impossible. After some minutes I have realized that that the compilation was successful, only the Problem window works erratic.
It is extremly frustrating.
How I got here:
- Clean project (and clean Problem Window manually by Ctrl+a and Del)
- Click on some other source file's tab (MyProtection.c and main.c) --> Errors appear !!!
It is a bug in CCSv6. The same was reported for earlier versions. Now the situation looks worse.