Hello.
I've developed my own RM57 board with CCS 6.0.1. It has worked until few hours ago..I changed some codes and build it, then I cannot write it to flash in RM57..I can't start debug mode.
Progress of loading program is stop in '0' when I push the debug button. It will be close soon and I can see a message as "Load program Error. File:C:\path\projectname\Debug\projectname.out: Load failed."
These are Console messages.
CortexR5: GEL Output: Memory Map Setup for Flash @ Address 0x0CortexR5: GEL Output: Memory Map Setup for Flash @ Address 0x0 due to System Reset
CortexR5: Flash operation timed out wating for the algorithm to complete. Operation cancelled.
CortexR5: GEL: File: C:\path\projectname\Debug\projectname.out: Load failed.
CortexR5: Trouble Removing Breakpoint with the Action "Remain Halted" at 0x8000080: (Error -1066 @ 0x8000080) unable to set/clear requested breakpoint. Verify that the breakpoint address is in valid memory. (Emulation package 5.1.507.2)
CortexR5: Unable to terminate memory download: NULL buffer pointer at 0x3a9f
CortexR5: GEL Output: Memory Map Setup for Flash @ Address 0x0 due to System Reset
Please help me.
+) I've tested latest version of my project operated well again, but there is a same problem.. I guess it is not a code problem..