Hi,
I am programming a camera based on a TMS320C64xx DSP. I've never had any problems with it. But in the last couple of days I've encountered a problem which I can't solve.
After calling a function from a libary I've started to receive the following warning:
entry point other than _c_int00 specified C:\ti\myprojects\Streaming\Release>rem @echo on C:\ti\myprojects\Streaming\Release>rem Remove debug info C:\ti\myprojects\Streaming\Release>C:/ti/\bin\strip6x Streaming.out C:\ti\myprojects\Streaming\Release>rem create .msf file C:\ti\myprojects\Streaming\Release>copy Streaming.out exec.out 1 Datei(en) kopiert. C:\ti\myprojects\Streaming\Release>C:/ti/ccsv4\vctools\util\econv32 Streaming econv version 1.0 - win32 supports vc/rt version 4.0 for TMS62Cxx systems file name too long C:\ti\myprojects\Streaming\Release>C:/ti/ccsv4\vctools\util\scvt32 scvt version 2.0 - win32 Streaming line 0 1411046047130 11463
Before that I've already had a warning ("entry point other than _c_int00") but it never made any troubles.
The new warning doesn't depend on the actual function because sometimes the warning disappears and then appears when I call another function. I've set up a small "hello world" programm and called the same troublemaking functions. One time it worked the other it didn't. I''ve spent already several hours to find the error but I can't finish my programm because this warning doesn't allow me to execute it. If the compiler produces this warning my program doesn't work anymore. I get the following error message from my os:
"Undefinde external symbol !!! fatal error, can't load program - fd:test.exe"
Probably someone has an idea how I can solve this problem!
Thank you in advance