Hello all,
Platform: Linux
CCS: 5.3.0.00090
I'm having a problem building multiple projects with the command line build. The command line build works fine on a windows platform, but when I try the same commands on a linux platform, the build hangs after building the external dependancy. the command syntax is
./eclipse -noSplash -data "$TI_Build_Workspace" -application com.ti.ccstudio.apps.projectBuild -ccs.projects <external_dependancy_name> <main project_name> -ccs.configuration Debug -ccs.buildType full -ccs.autoOpen`;
The external depency is built correctly, I can see the *.lib file in the correct location, but the main project build hangs and never returns.
I added the patch suggested in https://e2e.ti.com/support/development_tools/code_composer_studio/int-code_composer_studio/f/90/p/232908/845652.aspx?Redirected=true#845652 but I still see the same problem.
Regards