OS : Windows 7 32bit
CCS version : 5.4.0
MCU : TM4C1292NCPDT
Debuger : XDS560 STM (spectrum digital)
hi I am Graduate student.
I design digital board and it's MCU is TM4C1292NCPDT
i want test board design is right, so I need JTAG. my lab have XDS560 STM, i want use it.
but it is not work. error message is like this.
[Start]
Execute the command:
%ccs_base%/common/uscif/dbgjtag.exe -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity
[Result]
-----[Print the board config pathname(s)]------------------------------------
C:\Users\GINAND~1\AppData\Local\.TI\693494126\
0\0\BrdDat\testBoard.dat
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 560/2xx-class product.
This utility will load the program 'sd560v2u.out'.
E_RPCENV_IO_ERROR(-6) No connection: DTC_IO_Open::dtc_conf
Download failed for file C:\ti\ccsv5\ccs_base\common\uscif\xds560v2.out
An error occurred while soft opening the controller.
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver or utilities.
The value is '-250' (0xffffff06).
The title is 'SC_ERR_ECOM_EMUNAME'.
The explanation is:
An attempt to access the named emulator via USCIF ECOM has failed.
[End]
and i think it may be reason why it is not work.
it is my setting
how can I XDS560 is work?