I recently upgraded from Code Composer 4 to 6. Since then, I have not been able to always automatically run anything in the background. I have this feature set in Windows->Preferences->General, and this setting is being remembered. But every time I first start it up and build something, it always shows the pop-up. I set "Always run in background" and it will run in the background for the rest of the session. However, it always shows the pop-up when I start debugging. It also always checks for updates every time I start Code Composer, even though I ask it not to.
I had a difficult installation because our corporate IT will not allow disabling the virus scanner under any circumstances. Between the local IT guy and myself, we were eventually able to get it installed by performing some tricks. This problem may be the result of some security setting. I gave the program and all of its components full control, but I may have missed something.
So, what do I need to look at to find out why these settings are not being remembered?