Hello,
The original BeagleBone White has on-board JTAG shared with serial port via one USB port using FTDI chip.
I created CCXML file for the board with device AM3358 and had successful test connection.
But I'm NOT able to start debug due to error below
Error connecting to the target:
(Error -1266 @ 0x0)
Device is held in reset. Take the device out of reset, and retry the operation.
(Emulation package 5.1.232.0)
I have years of experience using this tool for AM1808 & OMAP. I can start debugging once I have a successful test connection for the JTAG ONLY IFF I set jumper on my board to DEBUG mode.
What should I do with this BB White !?!?
I'm using CCS-5.5 on Win7 PC
I also add AM335x_beaglebone.gel to the project