I must be missing something here. We develop extensively on C5000 family of devices (C5515,C5502,C5535 etc). The highest version of DSP-BIOS available for these devices seems to be 5.42.
In CCS v6 it appears that RTDX support has been removed and that the old legacy RTA that was available in CCS 5.5 via "tools\RTOS Analyzer\RTA(legacy)" just doesn't appear in the dropdown menu.
The CCS v6 documentation on the RTOS analyzer is based on the use of the "UIA" object/module and the section on configuring the logger type mentions that JTAGRUNMODE is available for only C6x devices. So it would seem "stop mode" is the only option available to us on the C5xxx.
Furthermore, because we need to use DSP-BIOS 5.42, which doesn't have a "UIA" module, it would seem that there is no way to get any instrumentation or run-time analysis information when using CCS v6 on a C5000 platform using DSP-BIOS 5.42.
Is this really the case? If so, it would seem that CCS v6 is not a suitable tool to develop/debug/profile DSP BIOS based applications on a C5000 part and we are better off staying with CCS v5.5. Do you agree?
Asked specifically, "How do I get RTA on a C5000 platform within CCS v6?"