with Blinky SDK example. The problem is I don't really know how to create the configuration file in Uniflash. The HTTPSERVER example does program and work but it has a preexisting configuration file. In the case of the Blinky example I create a new configuration file and a lot of stuff shows up automatically and I'm not sure what to do with it all. I add the blinky.bin file and it appears to program but it doesn't flash the leds.
Here's the links in the configuration file with the last entry new file being the Blinky.bin file