Hi, Everyone
I need your help.I use TM4C129x.
I wanna set .ID section to the end of used Flash area.
My Liker Command File is like this .
==============================
MEMORY
{
/* Application stored in and executes from internal flash */
FLASH (RX) : origin = APP_BASE, length = 0x00010000
/* Application uses internal RAM for data */
SRAM (RWX) : origin = 0x20000000, length = 0x00040000
}
/* Section allocation in memory */
SECTIONS
{
.intvecs: > APP_BASE
.text : > FLASH
.const : > FLASH
.cinit : > FLASH
.pinit : > FLASH
.init_array : > FLASH
.ID : > FLASH <--------I wanna set this Section to the end of used FLASH
.vtable : > RAM_BASE
.data : > SRAM
.bss : > SRAM
.sysmem : > SRAM
.stack : > SRAM
}
==============================
I do not want to fix address for .ID section.
Because I wanna make sure used Flash when we do update.
Do you have any idea?
Best regards
Hiroyasu