Dear all,
I´m having an old project buid with CCS version 2.21.13. It is code for a custom board. I have tried to convert this project into CCS version 6 using the legacy CCSv3.3 projects selection but this gives me a lot of trouble. The board has a mounted TMS320C2812. One of the first things I noticed was the need for an old xdctool package in order to the processor to be recognized 3.25.6.96. But now I get a lot of other error like the one shown below. I must admit that I´m fresh with respect to using CCS.
Can anyone give me some hints what the best way is to tackle this conversion step
Thanks in advance
Wim
Compilation failure
'Building file: ../app.cfg'
'Invoking: XDCtools'
"C:/TI/xdctools_3_25_06_96/xs" --xdcpath="C:/TI/xdais_7_24_00_04/packages;C:/TI/xdais_7_24_00_04/examples;C:/TI/ccsv6/ccs_base;" xdc.tools.configuro -o configPkg -t ti.targets.C28_large -p ti.platforms.concertoC28:TMS320C2812 -r debug -c "C:/TI/ccsv6/tools/compiler/c2000_6.2.7" "../app.cfg"
configuring app.x28L from package/cfg/app_p28L.cfg ...
error: ti.platforms.concertoC28.Platform: "C:/TI/xdctools_3_25_06_96/packages/ti/platforms/concertoC28/Platform.xs", line 179: ti.platforms.concertoC28.Platform.Instance#0 : ti.platforms.concertoC28 was passed unrecognized device name: 'TMS320C2812'.
js: "C:/TI/xdctools_3_25_06_96/packages/xdc/cfg/Main.xs", line 153: Error: Configuration failed!
xdctools_3_25_06_96\gmake.exe: *** [package/cfg/app_p28L.xdl] Error 1
js: "C:/TI/xdctools_3_25_06_96/packages/xdc/tools/Cmdr.xs", line 51: Error: xdc.tools.configuro: configuration failed due to earlier errors (status = 2); 'linker.cmd' deleted.
gmake: *** [configPkg/linker.cmd] Error 1
gmake: Target `all' not remade because of errors.