Hello,
I try to update the TIVA from UART with the help of UARTBootloader, It failes somehow.
but next time, when I flash the image of TIVA using JTAG,
It is giving me the following error:
Error connecting to the target:
(Error -1265 @ 0x0)
Device ID is not recognized or is not supported by driver. Confirm device and emulator configuration is correct, or update device driver.
(Emulation package 5.1.232.0).
The board seems to dead now.
Please suggest, what could be the possible issue ?
Thanks,
Sanchit Mehra