How can I generate a single makefile which has all the compiler options linker options etc. and has all depandancies without any includes which can be used by a thirdparty tool to build the project.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
How can I generate a single makefile which has all the compiler options linker options etc. and has all depandancies without any includes which can be used by a thirdparty tool to build the project.
When you tell CCS to auto-generate makefiles, it generates a main makefile and several *.mk include files.
http://processors.wiki.ti.com/index.php/Projects_and_Build_Handbook_for_CCS#Project_Files_and_Build_System_Overview
If you can provide them all the project metadata files (.project, .cproject and .ccsproject) then they can also build from command line without the need for CCS.
http://processors.wiki.ti.com/index.php/Projects_-_Command_Line_Build/Create
However, there is no automatic way to generate a single self-contained makefile. You would need to create this manually if that is what you desire.