Hi
I am using CCS 6.0.1.00040 .I am trying to built the example from https://2lemetry.atlassian.net/wiki/display/KB/Connecting+to+ThingFabric+with+a+Texas+Instruments+CC3200
i made the git clone as described and imported the project and built it,got error for gpio_if.c,i2c_if.c,uart_if.c similar like this
gmake: *** No rule to make target `C:/ti/CC3200SDK/cc3200-sdk/example/common/uart_if.c', needed by `uart_if.obj'.
as i checked it the path specified is wrong ,TI now adds a version number to the CC3200SDK install location - e.g. CC3200SDK_1.0.0
so the thingfabric project needs to be updated to reflect this.I changed the path as needed by right clicking the project and Properties->resource,
changed the CC3200SDK_INSTALL variable to C:\ti\CC3200SDK_1.0.0\cc3200sdk.
Now i built it and got following errors
#20 identifier "UINT8" is undefined main.c /thingfabric line 494 C/C++ Problem
#20 identifier "SL_NETAPP_HTTPPOSTTOKENVALUE" is undefined main.c /thingfabric line 492 C/C++ Problem
#20 identifier "ptr" is undefined main.c /thingfabric line 495 C/C++ Problem
#20 identifier "UINT8" is undefined main.c /thingfabric line 495 C/C++ Problem
#20 identifier "SL_NETAPP_HTTPGETTOKENVALUE" is undefined main.c /thingfabric line 443 C/C++ Problem
#20 identifier "SL_NETAPP_IP_LEASED" is undefined main.c /thingfabric line 285 C/C++ Problem
#20 identifier "ptr" is undefined main.c /thingfabric line 445 C/C++ Problem
#20 identifier "UINT8" is undefined main.c /thingfabric line 445 C/C++ Problem
#20 identifier "SL_NETAPP_IPV4_ACQUIRED" is undefined main.c /thingfabric line 274 C/C++ Problem
#20 identifier "SL_WLAN_SMART_CONFIG_START_EVENT" is undefined main.c /thingfabric line 238 C/C++ Problem
so i checked it,this implies it can't find something from the simplelink device library but that identifier isn't defined anywhere in the cc3200-sdk directory. Looks like my SDK is newer than that used for this sample code and that some of the identifiers have changed, e.g. SL_NETAPP_HTTPGETTOKENVALUE is now SL_NETAPP_HTTPGETTOKENVALUE_EVENT henceforth i changed all the identifiers to match of SDK 1.0.0.
again i built it,this what i got!!
#10008-D cannot find file "simplelink.a" main.c /thingfabric C/C++ Problem
#10008-D cannot find file "driverlib.a" main.c /thingfabric C/C++ Problem
#10010 errors encountered during linking; "thingfabric.out" not built main.c /thingfabric C/C++ Problem
<a href="file:/C:/ti/ccsv6/tools/compiler/dmed/HTML/10234.html">#10234-D</a> unresolved symbols remain main.c /thingfabric C/C++ Problem
i need help what do i do now?What causes the error?