HELP !
I imported a CS V3.1 project into CCS V5.2.
This is a DSP / BIOS project (V5.41.13.42)
I need to setup the memory via the Memory Section Manager.
How / Where do I do this?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HELP !
I imported a CS V3.1 project into CCS V5.2.
This is a DSP / BIOS project (V5.41.13.42)
I need to setup the memory via the Memory Section Manager.
How / Where do I do this?
donna famularo said:I need to setup the memory via the Memory Section Manager.
How / Where do I do this?
This is done in the DSP/BIOS Configuration Tool under System-.MEM - Memory Section Manager.
Please refer to the DSP/BIOS Users Guide for more information. If you have further questions I would suggest starting a new post in the TI-RTOS forum as the folks who monitor that forum have more expertise with DSP/BIOS.