Hello !
I was migrating to CCS v5 environment for MSP430 based project from IAR .During project development I required to change the output file name( < FileName 1>.txt)during compile time from the same sorce code.I was not able to find out where to do that. whereas it was easily done thru' IAR workbench by going thru' Linker > Output File at the time of compilation.In IAR the same project source file can be modified and a different .txt file can be generated w/o creating a new project.
In CCS i could see only "${BuildArtifactFileBaseName}.txt" option under "Properties >CCS Buid > Steps".
Plz let me know how to generate different output file name in CCS w/o creating a new project as per the intended file name.
Thanks,
ARS...