Hello:
Yesterday, I defined a 2-D vector with size 20*10 and my stack and heap size was the defaul value 0x400:
And I found that if I increase the size from 20 to 21 or 10 to 11, the system error occured.
Then I reset the stack and heap size as 0x5000 and 0x5000, I can define even vector[65][28] without error.
My confusion is that why the vector size has close connection with the stack and heap size?
If I want to create a very big matrix like vector[1000][100], I want to reset stack and heap size as 0x10000 and 0x10000 then the system refused me to set to this large value by reporting errors.
How to deal with this problem if I want to set a extremely large-sized vector?
Thank you
Yu