I swear it used to be I could import a CCS project from the examples directory without moving it into the workspace. I don't need two copies, I'm perfectly fine working with the one installed with the tools. I just notices that all the examples I imported with CCS v6.0 were relocated to the workspace. There is an option not to relocate files when I import but its selected and greyed out. What am I doing wrong. This used to be fairly intuitive.