HI
I want to plot two different variables in one graph only, so as to compare both the signals and check the delay between the input signal and transmitted signal.
I have gone through following post already:
But is of no use,as even dual time graph,i get the graphs on different plots so I can not observe the minute difference.
2. Is there any way by which I can get the voltage values sensed by adc to be plotted on DSO.
Thanks & Regards
Sneha