Hello,
I found the mistake to description of "Updating the XDS200 firmware" of wiki.
http://processors.wiki.ti.com/index.php/XDS200#Updating_the_XDS200_firmware
It is as follows exactly.
I download an update file from here and execute after saving on a local disk.
http://support.spectrumdigital.com/ccs51/RawPackages/sd_emupack_setup_5.2.0.13.exe
The update file of XDS200 is installed in the following folder.
"C:\ti\ccsv5\ccs_base\emulation\specdig\xds2xx\"
I execute by the command prompt of windows as follows.
1. Go to the folder where the update files:
C:\>cd "C:\ti\ccsv5\ccs_base\emulation\specdig\xds2xx"
2. Run the update batch file:
C:\ti\ccsv5\ccs_base\emulation\specdig\xds2xx>update_xds2xx.bat xds200
Regards, Hidetaka.