Dear TI support and forum members,
using ezdsp5502 and CCS 6.x on GNU/Linux Debian (jessie/testing), I'm experiencing since a while the following issue. After a sequence: run, pause, reset CPU, restart, the error occurs:
C55xx: GEL Output:
OnReset()
C55xx: GEL Output:
OnRestart()
C55xx: Trouble Setting Breakpoint with the Action "Finish Auto Run" at 0x26e90: (Error -1066 @ 0x26E90) Unable to set/clear requested breakpoint. Verify that the breakpoint address is in valid memory. (Emulation package 5.1.507.0)
C55xx: Breakpoint Manager: Retrying with a 55 Hardware breakpoint
Simple programs using DSP/BIOS are not affected.
I've checked, the stacks are big enough. What could be wrong in order to trigger such an error?
Thanks,
Andrey