I've got CCS v6.1.0 loaded on my Win-7 PC, but when I go to license it for the free 90-day eval (the first one, not the 2nd 90 day extension), I get an error code: 50016, Required file for activating required license is missing. Another funny thing is when I'm in the license manager in CCS6 -> License Information View -> Manage and try to check one of the boxes next to a license file location, I can do it, but it I do, then close the License Manager, reopen it and look again in Manage, the file is now unchecked. When I check a valid license file location (file from 03/23/15), then got to License Information View -> Upgrade -> Launch License Setup -> Evaluate -> Finish, I get the Error 50016. Is there something wrong with my .lic file from 3/23/15?
Please help me as currently, I only have a free license which doesn't let me use my emulator Signum JTAGJET-C2000 type.