Hello,
I have a CCSV5 project, for the DSK6713, which use to compile, build and run without issue. I unfortunately did an update on the tools, and it's never worked since. And the "revert" option in installation fails. The failure comes at the link, and is included below. I'm not sure where to start looking. Any advice or insight would be appreciated.
Regards,
Robert
<Linking>
"./workcfg.cmd", line 266: remark #10191-D: object ".printf" is not allocated,
"./workcfg.cmd", line 197: error #10099-D: placement fails for object
but is being placed as part of allocated object "GROUP_1"
.printf (COPY): {}
".hwi_vec", size 0x200 (page 0). Available ranges:
>> Compilation failure
IRAM size: 0x2fc00 unused: 0x3b8 max hole: 0x380
.hwi_vec: {
"./workcfg.cmd", line 289: error #10099-D: placement fails for object ".sts",
size 0x30 (page 0). Available ranges:
IRAM size: 0x2fc00 unused: 0x38 max hole: 0x1c
.sts: RUN_START(STS_A_TABBEG), RUN_START(_STS_A_TABBEG), RUN_END(STS_A_TABEND), RUN_END(_STS_A_TABEND) {
"./workcfg.cmd", line 221: error #10099-D: placement fails for object ".pinit",
size 0xf (page 0). Available ranges:
IRAM size: 0x2fc00 unused: 0x10 max hole: 0x8
.pinit: {} > IRAM
"./workcfg.cmd", line 237: error #10099-D: placement fails for object
".trcdata", size 0xc (page 0). Available ranges:
IRAM size: 0x2fc00 unused: 0x10 max hole: 0x8
.trcdata: {} > IRAM
"./workcfg.cmd", line 262: error #10099-D: run placement fails for object
".LOG_system$buf", size 0x100 (page 0). Available ranges:
IRAM size: 0x2fc00 unused: 0x0 max hole: 0x0
.LOG_system$buf: align = 0x100 {} > IRAM
"./workcfg.cmd", line 264: error #10099-D: placement fails for object
"GROUP_1", size 0xbb (page 0). Available ranges:
IRAM size: 0x2fc00 unused: 0x0 max hole: 0x0
GROUP {
"./workcfg.cmd", line 207: error #10099-D: run placement fails for object
".sem", size 0xb0 (page 0). Available ranges:
IRAM size: 0x2fc00 unused: 0x0 max hole: 0x0
.sem: {} > IRAM
"./workcfg.cmd", line 165: error #10099-D: run placement fails for object
".swi", size 0x84 (page 0). Available ranges:
IRAM size: 0x2fc00 unused: 0x0 max hole: 0x0
.swi: RUN_START(SWI_A_TABBEG), RUN_END(SWI_A_TABEND) {
"./workcfg.cmd", line 233: error #10099-D: placement fails for object
".gblinit", size 0x4c (page 0). Available ranges:
IRAM size: 0x2fc00 unused: 0x0 max hole: 0x0
.gblinit: {} > IRAM
"./workcfg.cmd", line 231: error #10099-D: placement fails for object
".switch", size 0x48 (page 0). Available ranges:
IRAM size: 0x2fc00 unused: 0x0 max hole: 0x0
.switch: {} > IRAM
"./workcfg.cmd", line 183: error #10099-D: run placement fails for object
".idlcal", size 0x4 (page 0). Available ranges:
IRAM size: 0x2fc00 unused: 0x0 max hole: 0x0
.idlcal: {
error #10010: errors encountered during linking; "work.out" not built
gmake: *** [work.out] Error 1
**** Build Finished ****