Yesterday I had a working version of CCSv6.1.0, then for unknown reasons I started having build failures related to the JVM not opening during tcf file build. Per the DSP/BIOS forum, I uninstalled, then re-installed CCS v6.1.0, followed by DSP/BIOS v5.42.1.09 & SYS/BIOS v6.41.02.41. I noticed right away in CCSv6 installed software that DSP/BIOS and SYS/BIOS are not in the list. This no longer seems to be a DSP/BIOS issue, but a CCS issue. In CCS Preferences->CCS->RTSC, the xdctools version is empty and if I click on it, there's no choice to select. In CCS->RTSC->Products, it does have TI-RTOS v2.10.1.38, and I tried manually adding paths to by DSP/BIOS v5.42.1.09 and then search but it found nothing.
One more thing. After re-installing CCSv6, there were two variable missing: 'RTDX_INCLUDE_DIR' & 'RTDX_LIB_DIR' whch couldn't be resolved. So I added them manually in the project build settings. This got rid of two warnings after build in the Problems view, but the error remains that CCS thinks DSP/BIOS v5.42 isn't installed. I've looked in C:\ti\bios_5_42_01_09 and it's all there and was re-installed after deleting this directory before the CCSvt6 re-install.
I'm stumped and very frustrated and need your help. Thanks.