Hello all,
I am trying to program TM4C123GH6PM using TivaWare. The only code I put in first is the include files:
#include <stdint.h> #include <stdbool.h> #include "inc/hw_memmap.h" #include "inc/hw_types.h" #include "driverlib/sysctl.h" #include "driverlib/gpio.h" uint8_t ui8PinData = 2;
When I tried to run it for the first time, it gave me an error about not finding hw_memmap.h . So I went in the project properties>Build>ARM Compiler>Include Options>Add dir... and added "C:\ti\TivaWare_C_Series-2.1.0.12573".
Now this error does not show up but these two started showing up:
error #10234-D: unresolved symbols remain
error #10010: errors encountered during linking; "lab3.out" not built
O tried to build the program at Project>Build Project but nothing.
What can I do to fix this?