- Using CCS.v6.1
- Dev Board DK-TM4C129X
- Installed examples according to instructions in http://www.ti.com/lit/ml/spmu352/spmu352.pdf
- refactored projects to my installed compiler TI v.5.2.3
- built all
When I start debugging by hitting F11 everything works fine. Example runs. I can even execute 'Run to Line' (crtl-R). Dev Board responds accordingly.
(Using Stellaris in-circuit debug interface)
When I set breakpoints they simply seem to be ignored by the execution! Execution always passes through the BP.
- Right clicking to insert a breakpoint or a hardware breakpoint always seems to insert a H/W BP.
- Disabling or enabling a BP has no effect
- BP type: Breakpoint, Skip count = 0, Conditon: empty, Action: Remain Halted (all defaults)
- The icon in the blue area to the left (next to the line with the BP) shows a blue bug which is crossed over with a single black line. I can't get this icon to change.