Hi all,
I've bee having some massive issues when it comes to linking files. Usually I would create a new project, and set it up as it is mentioned in the Workbook (Import vars.ini -> Add "%{TIVAWARE_INSTALL}" etc.). Now when it came to using other libraries that weren't in the standard install path (e.g. the buttons.h file) I would get errors that it is not linked, which I knew.
Therefore I decided to then import a project where I knew the file I wanted to was, and then set it up as mentioned in the Workbook. This is still giving me errors, and it constantly is stating it isn't linked. I've even moved the libraries I wanted to the "/inc/" to see if that would work, but that also gives me linking errors.
I'm at wits end here and getting very frustrated.