In the process of importing a CCS 3.3 project into CCS 5.5 it gives the error message:
"C:/vss_work/410037_DESULF/cmd/Gen00505b_dev.cmd", line 90: error #10100-D:
<Linking>
conflicting placement methods specified for ".text"
"C:/vss_work/410037_DESULF/cmd/Gen00505b_dev.cmd", line 90: error #10099-D: program will not fit into available memory. placement with alignment/blocking fails for section ".text" size 0x867e page 0. Available memory ranges:
>> Compilation failure
FLASHD size: 0x4000 unused: 0x0 max hole: 0x0
Here is part of the file containing the error(line 90 starts with .text :> ):
.reset : > RESET, PAGE = 0, TYPE = DSECT
IQmathTables : LOAD = BOOTROM, type = NOLOAD, PAGE = 0
IQmath : > FLASHB, PAGE = 0
csmpasswds : > CSM_PWL, PAGE = 0
csm_rsvd : > CSM_RSVD, PAGE = 0
codestart : > BEGIN_FLASH, PAGE = 0
vectors : > VECTORS, PAGE = 0, TYPE = DSECT
ramfuncs : LOAD = FLASHA,
RUN = PROG_LSARAM,
RUN_START(_ramfuncsRunStart),
LOAD_START(_ramfuncsLoadStart),
LOAD_END(_ramfuncsLoadEnd), align(128), PAGE = 0
DevelopmentFlash_A : > FLASHB, PAGE = 0
.esysmem : LOAD = LSARAM, align(128), PAGE = 1
CAN_Ram : LOAD = LSARAM, align(16), PAGE = 1
ControlRam : LOAD = LSARAM, align(16), PAGE = 1
OutbackRam : LOAD = MSARAM, align(16), PAGE = 1
SequencerRam : LOAD = H1SARAM, align(16), PAGE = 1
TempSeqRam : LOAD = LSARAM, align(16), PAGE = 1
AnodeFuelSeqRam : LOAD = H1SARAM, align(16), PAGE = 1
SystemSeqRam : LOAD = H1SARAM, align(16), PAGE = 1
LoadSeqRam : LOAD = H1SARAM, align(16), PAGE = 1
.bss : LOAD = LSARAM, align(16), PAGE = 1
.ebss : LOAD = H1SARAM, align(16), PAGE = 1
.text : > FLASHC >> FLASHD, PAGE = 0
.econst : > FLASHE, PAGE = 0
.printf : > FLASHA, PAGE = 0
.const : > FLASHA, PAGE = 0
.data : > FLASHA, PAGE = 0
.cio : LOAD = LSARAM, align(16), PAGE = 1
Development_PRAM : LOAD = H0SARAM, align(64), PAGE = 0
.switch : > FLASHE, PAGE = 0
.cinit : > FLASHB, PAGE = 0
.pinit : > FLASHB, PAGE = 0
THere probably is some difference between the way this file is read between CCS3.1 and CCS5.5 because this worked on the old version.
Any suggestions would be appreciated.
Thanks!