I converted a project from CCS3.1 to CCS5. The new CCS5 version of the project will build successfully and create an .out file which is then converted to a .rom. When I flash the .rom using our flash utility it wipes out the bootloader on the TMS320F2812. (Flashing the .rom generated via CCS3.1 works fine). Is there something I might have missed in the conversion from CCS 3.1 to 5?