Hello,
Sorry for the horrible title for this issue, but that's the best i could explain in such a short space.
I have a project with 2 build configurations and 2 different targets that are supposed to be running in parallel and I want to debug them simultaneously. Whenever I open the debug configurations and put the fixed path to each .out file in the "Program" field located in the "Program" tab the debugging process works perfectly. The thing is that I want to put this in a repository, so this file path cannot be fixed to my PC, it must have a relative path.
I tried using ${build_artifact:projectName}, since I read somewhere that this path changes depending on the build configuration it is configured for. Meaning that it should load the file located in the "build1/projname/projname.out" on the first microcontroller and then it should load the file located in "build2/projname/projname.out".
This doesn't happen. It loads only one build configuration into both microcontrollers (the first configuration). Could anyone help me?
This is my target configuration file:
And this is my debug configuration: