I have deleted the complete CC studio and reinstalled it about six times in the last few days. I shut it down, when I start up and try to debug the code I get the Load Program Error "Encountered a problem loading file; C:\
documents and Settings\Gil\workspace_v6_1\Blink The Led.out Could not open file.
If I do a new install it works a few times and I get the error. There are no errors shown except this one. The code is as follows: It has compiled and run several times. If I make a change or so it gives me that error. Undoing the change and/or inserting new code I get the same error.
This problem is consistent. It updated about an hour ago, the problem remains. I have had no system errors on this machine and other compilers work ok.
How do I fix it or do I go to another product?
//***************************************************************************************
// MSP430 Blink the LED Demo - Software Toggle P1.0
//
// Description; Toggle P1.0 by xor'ing P1.0 inside of a software loop.
// ACLK = n/a, MCLK = SMCLK = default DCO
//
// MSP430x5xx
// -----------------
// /|\| XIN|-
// | | |
// --|RST XOUT|-
// | |
// | P1.0|-->LED
//
// J. Stevenson
// Texas Instruments, Inc
// July 2011
// Built with Code Composer Studio v5
//***************************************************************************************
#include <msp430.h>
// Delay Function
doit( int x ) // Time is passed as X
{
volatile unsigned int i; // volatile to prevent optimization
do i = i-1; // Decrement by i
while(i > 0); // until zero is reached
return ; } // Finished nothing to return
int main(void) {
WDTCTL = WDTPW | WDTHOLD; // Stop watchdog timer
P1DIR |= 0x41; // Set P1.0 to output direction
for(;;) {
volatile unsigned int i; // volatile to prevent optimization
doit(30);
P1OUT ^= 0x00; // off
doit (20);
P1OUT ^= 0x40; // Red On
doit (3);
P1OUT ^= 0x01; // Red Green On
doit (30);
P1OUT ^= 0x40; // Green On
doit (30);
P1OUT ^= 0x01; // Red and green On
return 0;
}