Hello,
I am having issues debugging my project on the MSP430G2131. My circuit board is configured to use 4-Wire JTAG and I am very confident that the circuitry is correct. I referenced the MSP430 wiki at the following link: processors.wiki.ti.com/.../JTAG_(MSP430). At this point, I am stuck and don't know how to get this working. I am using the MSP-FET Flash Emulation Tool. I have tried reducing the "C1" value of the RST pin to comply with the max 2.2 nF recommendation. I have tried providing power externally and via the programmer but still nothing works...
Is there something I am missing on the project settings?
Any help would be greatly appreciated.
Thanks,
Adam