Hi All,
I would like to explore possibility to generate makefiles without using the eclipse. I am using Linux, is there a way to run TI makefile generation utility outside of eclipse?
Thanks...
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi All,
I would like to explore possibility to generate makefiles without using the eclipse. I am using Linux, is there a way to run TI makefile generation utility outside of eclipse?
Thanks...
Have you had a look at this wiki page for building from command line:
http://processors.wiki.ti.com/index.php/Projects_-_Command_Line_Build/Create
When I run
eclipse -noSplash -data /work/fw/ -application com.ti.ccstudio.apps.projectBuild -ccs.projects c1202-f5335
I get:
%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%% CCS headless build starting... [Mon May 04 14:55:32 EDT 2015] %%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%% ================================================================================ Pre processing... ================================================================================ Building... Gtk-Message: Failed to load module "overlay-scrollbar" **** Build of configuration Debug for project c1202-f5335 **** /home/sporty/ti/ccsv6/utils/bin/gmake -k all gmake: Nothing to be done for `all'. **** Build Finished **** ================================================================================ CCS headless build complete!
What do the "overlay-scrollbar" have to do with it?
Silver Diamond said:Gtk-Message: Failed to load module "overlay-scrollbar"
Perhaps the following links will be helpful?
https://bugs.launchpad.net/ubuntu/+source/overlay-scrollbar/+bug/1134202
http://blog.khmersite.net/2014/12/gtk-message-failed-to-load-module-overlay-scrollbar/