I'm running CCS v6.1 and have 4 inter-related projects. One is the master project, so that one has the other 3 as referenced projects. When building the master, the referenced ones seem to rebuild and link even if they were just built and have no changes. This is especially true when launching, the master goes on core 0 (I'm using a C6678) and the referenced ones are distributed over cores 1-5. Even if I launch twice in succession with no changes, it will rebuild all as indicated in the console window.
What process does CCS use in deciding when to build referenced projects? If it just does a make on all the referenced ones, why does make think things are not up to date? If I build the referenced projects individually, it seems to fix the problem, but I've not exhaustively tested it.
Mike