Hi,
I am using CCS 6.1 to run some examples on XEVMK2EX board.
The example is from TI Resource Explorer. The path is SYSBIOS/Unclassified Devices/66AK2E05/C66XX [C6000]/TI Target Examples/Minimal. I set the boot mode switches to '1111', and the project runs OK.
But the example for the ARM core failed to run.
The error message is:
arm_A15_0: Trouble Reading Memory Block at 0x80000000 on Page 0 of Length 0x4: (Error -1205 @ 0x80000000) Device memory bus has an error and may be hung. Verify that the memory address is in valid memory. If error persists, confirm configuration, power-cycle board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 5.1.641.0)
The example is SYSBIOS/Unclassified Devices/66AK2E05/Cortex A [ARM]/GNU Target Examples/Minimal.
Then I tried set the boot mode switches to '0010', and pressed key to stop autoboot in the U-Boot. After that, I started debugging the Minimal project. It is able to connect the ARM core, but the CPU didn't stop at main function.
I opened the targetConfigs/66AK2E05.ccxml, and I noticed that there is a .gel file for C66xx_0 core, but there is no .gel file for the ARM core.
My question is: do I need a .gel file for the ARM core? If so, is there any example file?
I am using Windows 7 64-bit, Service Pack 1.
CCS version: 6.1.0.00104
XEVMK2EX board version: v1.0.2.2 and I am using the onboard debug probe.
Thanks,
Xiuwen Cai